Other Parts Discussed in Thread: TMS320LF2407A
Hi,
I am working on TMS320LF2407A EVM. I know that it is not recommended for new development but please,i want you to help with this. I have followed the application note @ http://www.ti.com/lit/an/spra755a/spra755a.pdf . which was useful and i was able to execute the program mentioned in that AN.
I am trying to generate a sine wave using DAC on EVM. But when i tried to run the ISR generated by timer 1 (with no prescaling of clock) .The ISR is getting executed for 90+ times, after that the ISR is not executing. control is jumping to NMI ISR (happens when trying to access restricted memory). When the program is not accessing any restricted memory in first 90 ISR passes. How come it is accessing after 90 ISR executions.
The above problem is not occurring when i am prescaling the clock for timer1 by 128 times.
I am attaching the file the files..please look into the program.
0272.7178.cvectors.asm0755.4604.cos_ser.asm
/*********************************************************************
* Filename: example_c.c *
* *
* Author: David M. Alter, Texas Instruments Inc. *
* *
* Last Modified: 03/14/01 *
* *
* Description: This program illustrates basic initialization and *
* operation of the LF2407 DSP. The following peripherals are *
* exercised: *
* 1) Timer 2 is configured to generate a 250ms period interrupt. *
* 2) The quad LED bank on the LF2407 EVM is sequenced in the *
* Timer2 ISR. *
* 3) The IOPC0 pin is toggled in the Timer2 ISR. *
* 4) Timer 1 is configured to drive 20KHz 25% duty cycle symmetric *
* PWM on the PWM1 pin. *
* *
*********************************************************************/
/*** Address Definitions ***/
#include "f2407_c.h"
#define DAC0 port0000 /* EVM DAC register 0 (I/O space) */
ioport unsigned port0000; /* �24xx compiler specific keyword */
#define DAC1 port0001 /* EVM DAC register 1 (I/O space) */
ioport unsigned port0001; /* �24xx compiler specific keyword */
#define DAC2 port0002 /* EVM DAC register 2 (I/O space) */
ioport unsigned port0002; /* �24xx compiler specific keyword */
#define DAC3 port0003 /* EVM DAC register 3 (I/O space) */
ioport unsigned port0003; /* �24xx compiler specific keyword */
#define DACUD port0004 /* EVM DAC update register (I/O space) */
ioport unsigned port0004; /* �24xx compiler specific keyword */
#define DIPSWCH port0008 /* EVM DIP switch (I/O space) */
ioport unsigned port0008; /* �24xx compiler specific keyword */
#define LED port000C /* EVM LED bank (I/O space) */
ioport unsigned port000C; /* �24xx compiler specific keyword */
/*** Constant Definitions ***/
#define timer2_per 58594 /* 250ms timer2 period with a 1/128
timer prescaler and 30MHz CPUCLK */
#define pwm_half_per 80 /* period/2, 20KHz symmetric PWM with
a 30MHz CPUCLK */
/*#define pwm_duty 563 25% PWM duty cycle */
/*** Global Variable Definitions ***/
unsigned int LED_index; /* LED_index */
volatile unsigned int *pBank;
int sine_value;
/****************************** MAIN ROUTINE ***************************/
void main(void)
{
/*** Configure the System Control and Status registers ***/
*SCSR1 = 0x01FD;
*SCSR2 = (*SCSR2 | 0x000B) & 0x000F;
/*** Disable the watchdog timer ***/
*WDCR = 0x00E8;
/*** Setup external memory interface for LF2407 EVM ***/
WSGR = 0x0040;
/*** Setup shared I/O pins ***/
*MCRA = 0x00C0; /* group A pins */
*MCRB = 0xFE00; /* group B pins */
*MCRC = 0x0000; /* group C pins */
/*** Configure IOPC0 pin as an output ***/
*PCDATDIR = *PCDATDIR | 0x0100;
/*** Setup timers 1 and 2, and the PWM configuration ***/
*T1CON = 0x0000; /* disable timer 1 */
*T2CON = 0x0000; /* disable timer 2 */
*GPTCONA = 0x0000; /* configure GPTCONA */
sine_value = 0;
pBank = B0;
/* Timer 1: configure to clock the PWM on PWM1 pin */
/* Symmetric PWM, 20KHz carrier frequency, 25% duty cycle */
*T1CNT = 0x0000; /* clear timer counter */
*T1PR = pwm_half_per; /* set timer period */
*DBTCONA = 0x0000; /* deadband units off */
*ACTRA = 0x0006; /* PWM1 pin set active high */
*COMCONA = 0x8200; /* configure COMCON register */
*T1CON = 0x0840; /* configure T1CON register */
/* Timer 2: configure to generate a 250ms periodic interrupt */
*T2CNT = 0x0000; /* clear timer counter */
*T2PR = timer2_per; /* set timer period */
*T2CON = 0xD740; /* configure T2CON register */
/*** Other setup ***/
LED_index = 0x0001; /* initialize the LED index */
/*** Setup the core interrupts ***/
*IMR = 0x0000; /* clear the IMR register */
*IFR = 0x003F; /* clear any pending core interrupts */
*IMR = 0x0002; /* enable desired core interrupts */
/*** Setup the event manager interrupts ***/
*EVAIFRA = 0xFFFF; /* clear all EVA group A interrupts */
*EVAIFRB = 0xFFFF; /* clear all EVA group B interrupts */
*EVAIFRC = 0xFFFF; /* clear all EVA group C interrupts */
*EVAIMRA = 0x0080; /* enable desired EVA group A interrupts */
*EVAIMRB = 0x0000; /* enable desired EVA group B interrupts */
*EVAIMRC = 0x0000; /* enable desired EVA group C interrupts */
*EVBIFRA = 0xFFFF; /* clear all EVB group A interrupts */
*EVBIFRB = 0xFFFF; /* clear all EVB group B interrupts */
*EVBIFRC = 0xFFFF; /* clear all EVB group C interrupts */
*EVBIMRA = 0x0000; /* enable desired EVB group A interrupts */
*EVBIMRB = 0x0000; /* enable desired EVB group B interrupts */
*EVBIMRC = 0x0000; /* enable desired EVB group C interrupts */
/*** Enable global interrupts ***/
asm(" CLRC INTM"); /* enable global interrupts */
LED = LED_index;
/*** Proceed with main routine ***/
while(1); /* endless loop, wait for interrupt */
} /* end of main() */
/********************** INTERRUPT SERVICE ROUTINES *********************/
interrupt void timer1_isr(void)
{
float sine_scaled = 0;
*EVAIFRA = *EVAIFRA & 0x0080; /* clear T2PINT flag */
/*** Sequence the LED bank on the LF2407 EVM ***/
LED = LED_index; /* light the LEDs */
LED_index = LED_index << 1; /* left shift LED index */
if(LED_index == 0x0010) LED_index = 0x0001;
*PCDATDIR = *PCDATDIR ^ 0x0001;
sine_value = *pBank;
pBank = pBank+1;
if(pBank>(B0+95))
pBank = B0;
sine_scaled = sine_value/1000.0;
*CMPR1 = sine_scaled;
asm(" CLRC INTM");
}
Thanks in advance,
Raghu K