Other Parts Discussed in Thread: MOTORWARE
Hello, I have been evaluating an instaSpin FOC DRV8301-69M-KIT for a couple weeks. I have a question about what is used for the base value for the per unit values.
The confusion comes from conflicting documentation. The instaSpin users manual, section 5.1.2 seems to clearly state that the USER_IQ_FULL_SCALE_VOLTAGE_V
USER_IQ_FULL_SCALE_CURRENT_A are used as the base value.
Howerver the TI wiki clearly states that the TI DMC libraries use max measureable ADC values.
This is important to understand this because I want to re-scale the board to operate at 12 volt < 10 amp operating range. I have the hardware side figured out, I need to determine what all needs changed in the software.
Additional info:
I understand fixed point math and per unit values.
I'm using "proj_lab02a" that ships with Motorware as the source code to experiment with.
Thanks for any help.
- Steve