Other Parts Discussed in Thread: TMDSHVMTRINSPIN, MOTORWARE
Hello,
I tried to compare the Motor parameters with the one that Chris gave above also with the setting above that Chris mentioned for user.h.
I used the same motor (marathon 5K33GN2A) and TMDSHVMTRINSPIN (with F28069M). I ran GUI for InstaSPIN-MOTION and used Automatic ID (not from user.h) to identify my motor.
This is the result:
Compare to the identified values that Chris gave above, Rr of this motor is higher (56 ohm compared to 6 ohm).
Can you explain how this value is higher than the other (also the inductance is higher)? Can I use these parameter that I got to put in user.h?
Thank you.
Best regards,
Maria