Other Parts Discussed in Thread: UCC27324
Hello,
I'd like to have more info about the possibility of putting IN SERIES the output terminals of the dc/dc converters available in the kit. For example, I wish to buy 2 kits, to connect at their inputs two different PV panels and connect the output terminals of the two dc/dc converters available (one in the first kit and one in the second kit) in series, so that they share the current. The series connected terminals must be connected at a battery or to a constant voltage source. Thus, I wish to test a configuration used in Distributed MPPT applications.
The problem might be in the dc/dc converters controllers grounding, because the negative terminal of ONE dc/dc converter can be grounded, but not of both.
Please let me know if you need further details in order to give me a complete answer.
Thanks for your reply.
best regards
giovanni spagnuolo