This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 - Version of ROM Bootloader

Hello,

I refer to my earlier post: http://e2e.ti.com/support/microcontrollers/c2000/f/171/p/284617/996097.aspx#996097

I have another question concerning the ROM sources. At the moment there exist two versions, is there a possibility that there will be another version in the future for this DSP? If yes, how do I get the information if a bought device has a new version programmed?

I would need to know, if a new boot ROM version is used, because I have to define the SPI_boot function address to jump to.

Regards and many thanks,

Claudia