Hello.
I'm using C2000 Launchpad(LAUNCHXL-F28027, TMs320F28027PTT)
There was no problem before.
But suddenly, it gets stuck when I push reset button.
That time the PC address is 0x3FF5F5.
Before problem occurrence, I cut off some jumpers(jp4 ~ jp11), and tested the connection by multimeter.
After that the problem started.
I did't change anything in my code. Also, same problem occurs when I tested it by launchpad demo code.
Except the problem, the board works fine.
Why did the problem occur?
And, how can I solve that?