Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE
Hi guys.
In advance I apologize for the poor knowledge of the English language.
I'm working with TMS320F28335.
When i use Flash_Erase Api func, it comes back "1". For this Api func return codes are "0" if everything is all right, and from 20 to 24 if there is a mistake. I did all settings things that was written in datasheet (TMS320F2833x Flash API), but result was the same.
And when I call Api functions Flash_APIVersion and Flash_APIVersionHex, Flash_APIVersion returns "0" and Flash_APIVersionHex returns "3". I don't know why it's happens...
Has anyone see it before and what i need to do?
Thanx, Michael