Hi,
Please give the details of software and hardware connections for programming the 320F28027/35 controllers using SCI port. I don't want to use JTAG.
Regards
Toop
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Toop, there are several options here:
You can purchase a low-cost elprotronic FlashPro2000 flash programmer (programs via SCIA-BOOT mode - uses SCI RX, TX pins, a GND and possibly VDDIO pin)- http://www.elprotronic.com/flashpro2000.html Note this tool includes both JTAG AND SCI programming options.
You can use the free C2oooProg codeskin tool which programs via your RS232 connection. (http://www.codeskin.com/c2oooProg.html) Download link and Manual are on the left of that page.
Note, neither of these companies and solutions are affiliated with Texas Instruments, Inc.