Other Parts Discussed in Thread: MOTORWARE, DRV8301, DRV8312
Hi,
I'm using motorware 1.01.00.09 with CCS project "proj5g".
I'm trying to run my motor to 100RPM with INSTASpin FOC with some problems. I've read that in an other forum post that Chris suggested increasing Rs of 20-25%.
My motor parameters are:
Ls_d, Ls_q = 0.000202
Rs = 1.0
Flux = 0.02260
n poles = 2
With this configurations the motor not runs correctly at 100RPM, but if I set Rs = 1.25 (disabling Rs recalc) the motor runs considerably better.
Why it happens, even if the identification of the Rs is correct?
If I still increase the Rs value, how the motor runs?