Other Parts Discussed in Thread: TMS320F28069, CONTROLSUITE
Can't get interrupt with CPU Timer 0 working with TMS320F28069.
CpuTimer0Regs.TCR.bit.TIF sets to 1, and the interrupt is enabled with PieCtrlRegs.PIEIER1.all = 64, but won't vector to the ISR and PieCtrlRegs.PIEIFR1.all = 0, seeming to indicate that the interrupt flag didn't set.
This should be interrupt TINT0 at int1.7 in the PIE, hence the 64 (1000000b) for PieCtrlRegs.PIEIER1.all above.
I've successfully set up and used the 3 XINTs for a high-speed motor drive, but now need an interrupt from the timer to activate when timer count done at CpuTimer0Regs.TCR.bit.TIF = 1.
What's wrong here?
Thanks.