Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE, UNIFLASH
We have a program that works well on TMS320F28335 control board KIT when writing into RAM or FLASH (doesn't matter).
But when we are trying to install it into FLASH memory of the controller (it writes well into RAM memory) from our device, the compiler gives us an error:
"Flash operation timed out waiting for algorithm to complete. Operation cancelled"
The password in CSM is not installed: the Memory Browser window gives us FFFF FFFF FFFF FFFF at 0X33FFF8-0X33FFFF address.
Power supply of 3.3 V and 1.8 V performed similarly to KIT: each power pin of the controller is connected to the bus 3.3 V
and 1.8 V through a 100uH inductor and decoupling capacitor 0.1 uF 22uF in parallel. Supply voltage 3.3 V is delayed relative to the voltage 1.8 V.
Please help us to solve this problem. Is there any suggestions?