Hi,
I'm having trouble understanding how to setup the nominal values (current,velocity etc)
I think there 2 non-trivial situations:
1. You have the data from your manufacturer - But, when they say nominal current - is it RMS, is it peak.. rarely I think you get good information, and also then - which driver do they use ? different control methods will produce different values...efficiency of the drives...
2. You don't have any knowledge - what do you do ?
Passing through the labs, I think this is a crucial subject to pay high attention to, as many parameters in the software depends on that...
If you can suggest a way for identifying these nominal values for each motor it will be great... in that way, also each motor can be optimized, as manufacturing tolerances will also be taken into account...
I think that using information regarding the short-circuit current, R/L values can help this kind of procedure
thanks for your great support and effort !