Hi,
I am trying the USB_HOST_MSC example in the latest control Suite for F28M36 and it doesn't seem to be able to detect any of the USB memory sticks I'm trying to connect to the MicroUSB port through an adapter, new or old formatted on FAT16 or different format.
I am able to see the messages on the serial console but I'm always seeing NODEV cursor and if trying any of the commands FR_NOT_READY error code is returned.
I've noticed that somebody recommended to have USB0ID connected to ground and tried this too. Now I am able to see the LED light on some USB sticks but the program goes into a FaultISR loop.
I would like to know if anybody have had this kind of problem on a F28M36 control card (rev 1.1) or if it is any way to successfully run this example. All the other USB examples seem to be working fine from what I'm seeing.
Thanks
adis