This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCI FIFO timeout interrupt

Hi,TI expert!

C2000 SCI FIFO timeout feature is not available, if the number of bytes in FIFO cannot touch the FIFO level, it doesn't trigger the interrupt, in  fact , FIFO mode  cannot play the role of reducing interrupt frequency.  Why C2000 series can solve this issue?  I see  Stellaris® ARM® LM3S Microcontrollers can provide this feature, why C2000 doesn't?