This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using PFP package without PowerPad on PCB?

Hi all,

I'm developing a small control board with Piccolo 28069U and I've realized that could make my first version with a Sample from TI. The samples available are 28069PN (without PowerPad) and 28069UPFP (with USB+PowerPad). I would like to include the device with USB peripheral, but the free sample comes with PowerPad.

My question is: what could happen if I use the PFP package without any copper on PCB to dissipate heat? And, if I make a copper plane for the PowerPad but I don't solder it but I put thermal paste? Is it going to be better or worse than the PN package?


Many thanks!