Hi,
I've just been looking at the documentation which supports the 2833x Flash API, and there is a cautionary note regarding flash integrity, which says "... the device should always be programmed at the fastest possible CPU frequency. For example if the CLKIN frequency is 30 MHz, program the device at 150 MHz rather than 30 MHz or 60 MHz."
Does anyone have any information regarding the kind of tradeoffs which would be made by not programming at 150MHz? For example, does this reduce the number of erase \ programming cycles which can be undertaken, or reduce the reliability of the flash even if it's only programmed once at a lower frequency?
In our application, we don't have a fast enough input clock to scale up to 150MHz, but I don't have enough information to know whether I should panic or not!
Thanks in advance,
Simon