Other Parts Discussed in Thread: MOTORWARE
I want to do off-line simulation of instaSPIN-FOC. Do you done in simulink?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MOTORWARE
I want to do off-line simulation of instaSPIN-FOC. Do you done in simulink?
Hayaoki,
Currently we are not releasing the Simulink source for the FAST algorithm or InstaSPIN-FOC/-MOTION due to security/encryption concerns for our IP.
What we have released is
http://www.ti.com/tool/instaspinsim
Today this lets you choose from a selection of motors and then simulate with different speed/torque/load profiles.
Later this year it is being updated to allow you to enter your own motor parameters.
I don't have a date yet for the on-line simulation update. Probably November+.
Thank you for answer.
1: Is it possible to code generation and simulation if vissim
2: " http://processors.wiki.ti.com/index.php/InstaSPIN"
3-day VisSim based InstaSPIN ™ - FOC workshop
When will?
Thanks in advance.
1. Currently no, VisSim has not added the components necessary to populate the MotorWare user.h and use the proj_lab##.c as a template for code generation. There is a person working on this capability to enable the Workshop, but as it isn't TI I can't comment on the schedule.
2. We are probably going to run the first version by end of year in Europe. We are also waiting on the VisSim capability to be finalized/tested as well as some new hardware we would like to use for this class. I can't give an exate date on when it will spread broader but it should happen in 2014.