Other Parts Discussed in Thread: MOTORWARE
Hello,
I'm having a problem with instaSPIN-FOC when SpeedRef_krpm = 0.0. At the beginning the motor is stopped, but after a moment (seconds or minutes, that's depends) the motor is spinning around 200 rpm with the maximum current that is defined in user.h.
Of course, during this problem, SpeedRef_krpm stays at 0.0.
The flags in gMotorVars are set as below :
Flag_enableSys = true
Flag_Run_Identify = true
Flag_MotorIdentify = true
Flag_enableForceAngle = true
Flag_enableFieldWeakening = false
Flag_enableRsRecalc = false
Flag_enableUserParams = true
Flag_enableOffsetcalc = true
Flag_enableEpl = false
Thank you in advance,