Hİ,
I use 2 channel ADC would like to see one of the square wave triangle wave from the other. To do this, I used the following program.
Adc channel figure of a triangle wave applied first got here below (1.figure).However, the second ADC channel applied square wave, but I have a different shape from (2 figure).
Do I make mistakes ADC settings? Can you help please.
PROGRAM
#include "DSP2833x_Device.h"
// external function prototypes
extern void InitAdc(void);
extern void InitSysCtrl(void);
extern void InitPieCtrl(void);
extern void InitPieVectTable(void);
extern void InitCpuTimers(void);
extern void ConfigCpuTimer(struct CPUTIMER_VARS *, float, float);
extern void display_ADC(unsigned int);
void delay_loop(long );
// Prototype statements for functions found within this file.
void Gpio_select(void);
interrupt void cpu_timer0_isr(void);
interrupt void adc_isr(void); // ADC End of Sequence ISR
// Global Variables
unsigned int Voltage_VR1;
unsigned int Voltage_VR2;
unsigned int Voltage_VR3[1000];
unsigned int Voltage_VR4[1000];
unsigned int i=0;
unsigned int j=0;
unsigned int ADCokundu=0;
//###########################################################################
// main code
//###########################################################################
void main(void)
{
InitSysCtrl(); // Basic Core Init from DSP2833x_SysCtrl.c
EALLOW;
SysCtrlRegs.WDCR= 0x00AF; // Re-enable the watchdog
EDIS; // 0x00AF to NOT disable the Watchdog, Prescaler = 64
DINT; // Disable all interrupts
Gpio_select(); // GPIO9, GPIO11, GPIO34 and GPIO49 as output
// to 4 LEDs at Peripheral Explorer)
InitPieCtrl(); // basic setup of PIE table; from DSP2833x_PieCtrl.c
InitPieVectTable(); // default ISR's in PIE
InitAdc(); // Basic ADC setup, incl. calibration
AdcRegs.ADCTRL1.all = 0;
AdcRegs.ADCTRL1.bit.ACQ_PS = 7; // 7 = 8 x ADCCLK
AdcRegs.ADCTRL1.bit.SEQ_CASC =1; // 1=cascaded sequencer
AdcRegs.ADCTRL1.bit.CPS = 0; // divide by 1
AdcRegs.ADCTRL1.bit.CONT_RUN = 0; // single run mode
AdcRegs.ADCTRL2.all = 0;
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1; // 1=enable SEQ1 interrupt
AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 =1; // 1=SEQ1 start from ePWM_SOCA trigger
AdcRegs.ADCTRL2.bit.INT_MOD_SEQ1 = 0; // 0= interrupt after every end of sequence
AdcRegs.ADCTRL3.bit.ADCCLKPS = 3; // ADC clock: FCLK = HSPCLK / 2 * ADCCLKPS
// HSPCLK = 75MHz (see DSP2833x_SysCtrl.c)
// FCLK = 12.5 MHz
AdcRegs.ADCMAXCONV.all = 0x0001; // 2 conversions from Sequencer 1
AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0; // Setup ADCINA0 as 1st SEQ1 conv.
AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 1; // Setup ADCINA1 as 2nd SEQ1 conv.
//AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 2;
EPwm2Regs.TBCTL.all = 0xC030; // Configure timer control register
/*
bit 15-14 11: FREE/SOFT, 11 = ignore emulation suspend
bit 13 0: PHSDIR, 0 = count down after sync event
bit 12-10 000: CLKDIV, 000 => TBCLK = HSPCLK/1
bit 9-7 000: HSPCLKDIV, 000 => HSPCLK = SYSCLKOUT/1
bit 6 0: SWFSYNC, 0 = no software sync produced
bit 5-4 11: SYNCOSEL, 11 = sync-out disabled
bit 3 0: PRDLD, 0 = reload PRD on counter=0
bit 2 0: PHSEN, 0 = phase control disabled
bit 1-0 00: CTRMODE, 00 = count up mode
*/
EPwm2Regs.TBPRD = 2999; // TPPRD +1 = TPWM / (HSPCLKDIV * CLKDIV * TSYSCLK)
// = 20 µs / 6.667 ns
EPwm2Regs.ETPS.all = 0x0100; // Configure ADC start by ePWM2
/*
bit 15-14 00: EPWMxSOCB, read-only
bit 13-12 00: SOCBPRD, don't care
bit 11-10 00: EPWMxSOCA, read-only
bit 9-8 01: SOCAPRD, 01 = generate SOCA on first event
bit 7-4 0000: reserved
bit 3-2 00: INTCNT, don't care
bit 1-0 00: INTPRD, don't care
*/
EPwm2Regs.ETSEL.all = 0x0A00; // Enable SOCA to ADC
/*
bit 15 0: SOCBEN, 0 = disable SOCB
bit 14-12 000: SOCBSEL, don't care
bit 11 1: SOCAEN, 1 = enable SOCA
bit 10-8 010: SOCASEL, 010 = SOCA on PRD event
bit 7-4 0000: reserved
bit 3 0: INTEN, 0 = disable interrupt
bit 2-0 000: INTSEL, don't care
*/
EALLOW;
PieVectTable.TINT0 = &cpu_timer0_isr;
PieVectTable.ADCINT = &adc_isr;
EDIS;
InitCpuTimers(); // basic setup CPU Timer0, 1 and 2
CpuTimer0.InterruptCount=0;
ConfigCpuTimer(&CpuTimer0,150,10000); //100ms de bir int üretir
PieCtrlRegs.PIEIER1.bit.INTx7 = 1; // CPU Timer 0
PieCtrlRegs.PIEIER1.bit.INTx6 = 1; // ADC
IER |=1;
EINT;
ERTM;
CpuTimer0Regs.TCR.bit.TSS = 0; // start timer0
// DINT;
while(1)
{
delay_loop(1);
{
{
GpioDataRegs.GPASET.bit.GPIO13 = 1;
GpioDataRegs.GPASET.bit.GPIO11 = 1;
GpioDataRegs.GPASET.bit.GPIO17 = 1;
GpioDataRegs.GPASET.bit.GPIO25 = 1;
GpioDataRegs.GPASET.bit.GPIO27 = 1;
GpioDataRegs.GPASET.bit.GPIO19 = 1;
}
{
CpuTimer0.InterruptCount=0;
}
}
while(CpuTimer0.InterruptCount <1)
{
//wait for 500 ms
EALLOW;
SysCtrlRegs.WDKEY = 0x55; // Service watchdog #1
EDIS;
}
//Display VR1 voltage
display_ADC(Voltage_VR1);
while(CpuTimer0.InterruptCount <1) // wait for 1000 ms
{
EALLOW;
SysCtrlRegs.WDKEY = 0x55; // Service watchdog #1
EDIS;
}
// Display VR2 voltage
display_ADC(Voltage_VR2);
CpuTimer0.InterruptCount = 0;
}
}
//*******************************************************************
void delay_loop(long end)
{
long i;
for (i = 0; i < end; i++)
{
asm(" NOP");
EALLOW;
SysCtrlRegs.WDKEY = 0x55;
SysCtrlRegs.WDKEY = 0xAA;
EDIS;
}
}
//*******************************************************************
void Gpio_select(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX1.all = 0; // GPIO15 ... GPIO0 = General Puropse I/O
GpioCtrlRegs.GPAMUX2.all = 0; // GPIO31 ... GPIO16 = General Purpose I/O
GpioCtrlRegs.GPBMUX1.all = 0; // GPIO47 ... GPIO32 = General Purpose I/O
GpioCtrlRegs.GPBMUX2.all = 0; // GPIO63 ... GPIO48 = General Purpose I/O
GpioCtrlRegs.GPCMUX1.all = 0; // GPIO79 ... GPIO64 = General Purpose I/O
GpioCtrlRegs.GPCMUX2.all = 0; // GPIO87 ... GPIO80 = General Purpose I/O
GpioCtrlRegs.GPADIR.all = 0;
GpioCtrlRegs.GPADIR.bit.GPIO9 = 1; // peripheral explorer: LED LD1 at GPIO9
GpioCtrlRegs.GPADIR.bit.GPIO11 = 1; // peripheral explorer: LED LD2 at GPIO11
GpioCtrlRegs.GPADIR.bit.GPIO13 = 1;
GpioCtrlRegs.GPADIR.bit.GPIO19 = 1;
GpioCtrlRegs.GPADIR.bit.GPIO17 = 1;
GpioCtrlRegs.GPADIR.bit.GPIO25 = 1;
GpioCtrlRegs.GPADIR.bit.GPIO27 = 1;
GpioCtrlRegs.GPBDIR.all = 0; // GPIO63-32 as inputs
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1; // peripheral explorer: LED LD3 at GPIO34
GpioCtrlRegs.GPBDIR.bit.GPIO49 = 1; // peripheral explorer: LED LD4 at GPIO49
GpioCtrlRegs.GPCDIR.all = 0; // GPIO87-64 as inputs
EDIS;
}
interrupt void cpu_timer0_isr(void)
{
CpuTimer0.InterruptCount++;
EALLOW;
SysCtrlRegs.WDKEY = 0xAA; // service WD #2
EDIS;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
interrupt void adc_isr(void)
{
Voltage_VR1 = AdcMirror.ADCRESULT0; // store results global
Voltage_VR2 = AdcMirror.ADCRESULT1;
Voltage_VR4[i]=Voltage_VR2;
Voltage_VR3[i]=Voltage_VR1;
i++;
// Reinitialize for next ADC sequence
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1
AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear INT SEQ1 bit
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
}
//===========================================================================
// End of SourceCode.
//===========================================================================