Hello sir,
For my new project i am actively considering C2000 based Peak current controlled phase shift full bridge .In this regard i am referring the application note :"Implementing Phase Shifted Full Bridge DC - DC Converter with C2000 Microcontrollers",Hrishikesh Nene C2000 Systems and Applications Team,Version 1.1 – March 2012........
Question1: Refering to the Figure 12.PCMC PWM Waveforms , from the Q2 waveform,it is appearing as if the Q2,Q3 PWM is operating at a lower frequency compare to Q1,Q4 PWM especially when load peak current refernce is increased. It seems that when the peak current reference is increased Q2 turn on time increases beyond the Switching period/2. Suggesting a variable frequency operation for Q2,Q3 PWM is this my understanding is correct?
Question2: Figure 11.PCMC Block Diagram , the Ipri signal is derived from the ADC block which is shown as 100KHz. For peak current control the comparator has to actively trip the PWM switches for both positive half and the negative half cycle of the current waveform, which requires a sampling of 200kHz. However the diagram implies that the comparator is actively controlling the PWM only in one half cycle of the PWM period. Is my understanding correct ?
Regards
Meeravali