Hi
I have only recently got involved with the C2000 Piccolo devices thus I am a bit of a novice.
I was playing with a 28035 chip in the standard 100 pin TI development kit. Everything was going o.k and then suddenly the ccsv5 complained that it could not communicate with the emulator.
The following Blurb was shown on the ccsv5 console.
C28xx: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. (Emulation package 5.1.73.0)
I have run the xds100serial.exe, which resulted in:
VID/PID Type SERIAL# Description
0403/6010 blank EEPROM unknown no description available
What is the verdict?
Please Help
cheers Dave