Other Parts Discussed in Thread: TMDSDOCK28035
Hello all,
I am trying to use TMDSDOCK28035, piccolo experimenter's kit to run a three phase AC motor. Following is the code where I set the PWM outputs,
//set compare registers
EPwm1Regs.CMPA.half.CMPA = compValue[0]; //PWM 1A - PhaseA
EPwm1Regs.CMPB = compValue[1]; //PWM 1B - PhaseB
EPwm2Regs.CMPA.half.CMPA = compValue[2]; //PWM 2A - PhaseC
EPwm2Regs.CMPB = 0;
and these are sent to the GPIO pins using the following code
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // 0=GPIO, 1=EPWM1A, 2=Resv, 3=Resv
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // 0=GPIO, 1=EPWM1B, 2=Resv, 3=COMP1OUT
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // 0=GPIO, 1=EPWM2A, 2=Resv, 3=Resv
When I look at these pins on the scope, I see the PWM outputs but they have jitter, the edges seem to vary around 20us and PWM interrupt is running at a rate of 10khz. Because of this my mosfet gate drive outputs also has the same jitter. How can I avoid this?
Appreciate any inputs.