This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A question about lnk.cmd ?

Other Parts Discussed in Thread: TMS320F28035

hello,

i am using c28035 these days, some documents says it has about 10KB ram , .

I found that

.init needs about 3K,

.text  needs about 6K,

.ebss needs about 3K,

it may not have sufficient place any more.

So  can i put (.init) into boot ROM ? like that:

ROMINIT   : origin = 0x3FE000, length = 0x000900   

.cinit           : > ROMINIT,     PAGE = 0            /*check*/     

------------------------------------------------------------------------------

The initialized variables are stored in the .cinit . And the .ebss is reserved for global varibles .

After power on , data in .cinit  is copied into .ebss.  Then the place in .cinit is empty .

so can I use the place in .cinit again ? because the place is useful , 

  the figure is 28035  memory map.