Other Parts Discussed in Thread: UNIFLASH
Hi,
28335 controller was working well on my board till last week. This board has been working from a year without any issue. After rearrangement of my set up (without any changes on the controller board), i found that the controller is unable to use flash. When i load the code, ccs stuck in the erasing (i waited for 5 mins). Then i aborted the operation and when again tried to load, it shows flash is locked. Later i replaced the controller with new controller. The same issue i observed with the new controller in the same board.
Then to verify whether the problem is in the controller or board, i used the removed controller IC in the eZDSP evaluation board, and worked well.
I want to know what could have been the issue occurred in my board which is stopping me to flash? I checked the voltages, 3.28V and 1.88V on the board.
Thanks,
Kartik Brahmbhatt
Honeywell