Other Parts Discussed in Thread: MOTORWARE, DRV8312
Hello
i m using the last version of motorware , compiler ..
on a Drv8312 kit with the bly172s motor
in the FOC example lab03b , i can turn slowly , identify the motor.. but if i try to increase the speed, the current increase and the speed cannot go above 1800 rpm (with 24 volt)
all the others examples labxxx have also the same probleme
with the GUI instaspin application there is not this probleme and i can go to 3200 rpm without field weakenning.
ALL the labs with fpu32 (labs03c for exemple ) doesn not work (the motor doesn't turn )
can you help me ?
thanks
karim chraibi