This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI Chip Select does not pull down

Hi, 

I am trying to get the SPI working on one of my setups.

The SPI master is C2000- F28027 device. And I am using one of the booster packs as SPI slave. 

I am using the sample example 'spi_loopback' as the reference. When I try to execute this with my booster pack, I see that the chip select (J2.3) does not pull low. Because of this C2000 device is not able to communicate with the slave.

I tried to execute this example stand-alone, i.e, without any booster packs connected to it. I can still see the same behavior. 

Please give some inputs.

Thanks & Regards,

Raghavendra