This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problems with 28335 interrupts

i am trying to generate gating pulses with f28335. i am struggling with interrupts. without interrupts it is working but by using interrupts it is not working. i think i am doing wrong with initilaisation of ISR. here i am attaching my code.please help me.


#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

// Prototype statements for functions found within this file.
void InitEPwm1Example(void);

interrupt void epwm1_isr(void);


void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
   InitSysCtrl();

// Step 2. Initalize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();  // Skipped for this example

// For this case just init GPIO pins for ePWM1, ePWM2, ePWM3
// These functions are in the DSP2833x_EPwm.c file
   InitEPwm1Gpio();
   InitEPwm2Gpio();
   InitEPwm3Gpio();

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
   DINT;

// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
   InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
   IER = 0x0000;
   IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
   InitPieVectTable();

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
   EALLOW;  // This is needed to write to EALLOW protected registers
   PieVectTable.EPWM1_INT = &epwm1_isr;
   EDIS;    // This is needed to disable write to EALLOW protected registers

// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals();  // Not required for this example


   EALLOW;
   SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
   EDIS;

   InitEPwm1Example();
   
   EALLOW;
   SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
   EDIS;


// Enable CPU INT3 which is connected to EPWM1-3 INT:
   IER |= M_INT3;

// Enable EPWM INTn in the PIE: Group 3 interrupt 1-3
   PieCtrlRegs.PIEIER3.bit.INTx1 = 1;
   PieCtrlRegs.PIEIER3.bit.INTx2 = 1;
   PieCtrlRegs.PIEIER3.bit.INTx3 = 1;
   PieCtrlRegs.PIEIER3.bit.INTx4 = 1;
   PieCtrlRegs.PIEIER3.bit.INTx5 = 1;
   PieCtrlRegs.PIEIER3.bit.INTx6 = 1;
   
    
// Enable global Interrupts and higher priority real-time debug events:
   EINT;   // Enable Global interrupt INTM
   ERTM;   // Enable Global realtime interrupt DBGM



// Step 6. IDLE loop. Just sit and loop forever (optional):
   for(;;)
   {
       asm("          NOP");
   }

}

interrupt void epwm1_isr(void)
{
	
	

   // Clear INT flag for this timer
   EPwm1Regs.ETCLR.bit.INT = 1;

   // Acknowledge this interrupt to receive more interrupts from group 3
   PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
   
   // Setup compare
   EPwm1Regs.CMPA.half.CMPA = 1000;

 }


void InitEPwm1Example()
{

   EPwm1Regs.TBPRD = 2343;                        // Set timer period
   EPwm1Regs.TBPHS.half.TBPHS = 0x0000;           // Phase is 0
   EPwm1Regs.TBCTR = 0x0000;                      // Clear counter

   // Setup TBCLK
   EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
   EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;        // Disable phase loading
   EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0x2;  //TB_DIV4;       // Clock ratio to SYSCLKOUT
   EPwm1Regs.TBCTL.bit.CLKDIV = 0x3;   //TB_DIV4;

   EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;    // Load registers every ZERO
   EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
   EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
   EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

     // Set actions
   EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;             // Set PWM1A on Zero
   EPwm1Regs.AQCTLA.bit.CAD = AQ_SET;


   EPwm1Regs.AQCTLB.bit.CAU = AQ_SET;          // Set PWM1B on Zero
   EPwm1Regs.AQCTLB.bit.CAD = AQ_CLEAR; 

}


//===========================================================================
// No more.
//===========================================================================