Hello,
I'm using the 28335 and I am trying to implement a eCAN listen-only mode.
The idea is to listen to the CAN bus without disturbing any (!) running communication.
In case of one special CAN message I would like to stop the listen mode and start to communicate.
Did anybody already implement something like this?
Thank you for every hint!
Regards,
Roger
Note that a initialization of the eCAN with the wrong bit rate will disturb a running communication, even if I do not send anything!
A auto-baud function for eCAN would also solve my problem...