Other Parts Discussed in Thread: TMS320C28346
Hello,
I am looking for a part more powerful (in speed and RAM) than the F28335. The TMS320C28346 has more RAM and runs at 300 MHz, which is an improvement if compared with the F28335.
It seems that this the only option within TI, to have a faster device with an internal PWM peripheric for motor control (with the exception of some old parts of the OMAP familiy). The Concerto CPU parts cannot run faster than 150 MHz, and the ARM cannot help on this task.
Besides the TMS320C28346, there is any suggestion?
Your comments are welcome.
Thank you,
Oscar