Other Parts Discussed in Thread: UNIFLASH
Hi,
I am working with 28335. I interface it with the Nexys2 Spartan 3E DSP. It was working fine till today. But, today evening when I changed some connections, it suddenly started giving me error message while programming dsp. The exact error message is as follows.
"C28xx: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. (Emulation package 5.1.232.0)"
When I removed all the external connections, it again started working.
I want to know the reason of the problem and solve it. Pl. help me. I feel the USB cable is not faulty. So, there may be some mistake in connections. But I don't understand exactly what is the mistake. (I am using GPIO0-34 and GPIO 60 only outof all available for external connections ) Iwant to know the reason of the problem so that it don't get repeated.
More over for testing the USB cable as mentioned in the message I tried to find out the utility 'common/uscif' which I could not find. So, what is the exact location of the command line utility?
Pl. reply me.
Vipul Patel