Hi all,
I'm using a modified DMC example project (HVPM Sensored) with my F28335 on a TMSDOCK with the XDS100 USB emulator. Power circuits are custom built.
I want to display graphs like written in the documentation, for example the output of the ramp generator module. First thing that makes me wondering is, that in my watch window nearly every variable is displayed as a "float" type in "natural" format. I even can't set the correct Q value. When right clicking on the variable the "Q-Value" entry is disabled. In the documentation most values are "long" type. What could cause this problem?
As far as I understand, I can only display graphs from the Datalog module. So I tried to display the start adresses DlogCh1 to DlogCh4. But the results are just rubbish.
This an example where I tried to display rg1.Out which is connected to DlogCh2. The motor was disconnected.
I hope you guys can help me in this case.
Thanks
Philipp