This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XINTF - Can I use XA lines as GPIO when using XINTF



On an F28335 I want to connect a parallel ADC up (TI ADC8422) via the XINTF. This is the only memory device connect edand I plan to trigger ADC conversions via one of the ePWMs and then use DMA to transfer the data when the conversion complete line on the ADC goes low (/BUSY). I don't need to use any of the XA address lines to access the ADC. My question is, can I configure the XA lines to be normal GPIO when using the XINTF?  Thanks.