Other Parts Discussed in Thread: TMS320F28232
Dear All:
I'm using TMS320F28232 .
There are some assembly codes as follows:
FunArray:
.long Fun1 ;
.long Fun2;
.long Fun3;
.long Fun4;
MOVL XAR2, #FunArray
MOVZ AR0, #1
MOVL XAR7, *+XAR2[AR0]
LCR *XAR7
MOVZ AR0, #3
MOVL XAR7, *+XAR2[AR0]
LCR *XAR7
These codes are used to allocating some application funcitons. AR0 is the index. #FunArray is the entry for all allocated functions, which are unified as an array.The address of allocated function is long type. So, the index should be an even number, but not odd.
Although, in the former code, the index is exactly an odd number, and and the codes can run correctly ,which means that the code can allocate the correct address and find the correct funcion entry.
I'm puzzle very much. I'm looking forward to your help. Thank you very much!
Your sincere
Andrew Xiao