Other Parts Discussed in Thread: CONTROLSUITE, TMDSCNCD28069ISO
Hello TI,
Is the USB version of the TMS320F28062U available?
Thanks!
johnw
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CONTROLSUITE, TMDSCNCD28069ISO
Hello TI,
Is the USB version of the TMS320F28062U available?
Thanks!
johnw
Hi John!
Perhaps you are looking for it
ti\controlSUITE\device_support\f2806x\v136\F2806x_examples_ccsv5\usb_....
\ti\controlSUITE\device_support\f2806x\v136\MWare\usblib\
Regards,
Igor
Hello Igor,
What I mean is the hardware reference design schematics for the internal USB port of the 'U' devices.
Thanks!
johnw
You can refer to SPRUH18D 3755.TI_TMS320x2806x_TRM.pdf (p.1108). Also maybe this link will be useful http://e2e.ti.com/support/microcontrollers/c2000/w/design_notes/usb-thoughts-on-2806x-usb-design-considerations.aspx
Regards,
Igor
John,
The F28069 ISO controlCARD has hardware that works with the F28069's USB peripheral and should serve as a good reference.
Its schematics can be found within controlSUITE at:
\controlSUITE\development_kits\~controlCARDs\TMDSCNCD28069ISO_v1_0\R0_3\
Thank you,
Brett
Hello Brett,
I will take a look at that - and I want to order some of these (TMS320U28069U's).
Stock seems a little on the lite side where I have checked.
Thanks!
John
Brett,
OK - the FTDI 2232H is there for the XDS Emulation - and I see on page 3 where GPIO_26 and GPIO_27 are D+ and D- and that's a decent reference for the USB. That's what I was looking for.
Can I use XDX-100v3 for the '69U? I will review all 3 of those to see which one is best.
Thanks!
John
Hi,
Can I use XDX-100v3 for the '69U?
Yup, you can; XDS100v2 can also be used.
Regards,
Gautam
Thanks Gautam,
Interesting you can't seem to order the TMDSCNCD28069ISO right now on the eStore even though on the C28x pages it is showing as active.
Regards,
johnw