Other Parts Discussed in Thread: CONTROLSUITE
Hi all,
I'm using Piccolo TMS320F28069PU device and trying to use HRPWM peripheral. First of all, I've read all the proper documentation about this peripheral and have run the "hrpwm_prdup_sfo_v6" example from ControlSuite. In this case, it's all fine.
But I have problems while trying to compile my own code. Previously, I used ePWM (whithout high-resolution) and it worked perfectly. I copied some functions from the TI project example and included SFO_V6.h file and SFO_TI_Build_V6b_FPU.lib to my project. I also include rts2800_fpu32.lib But now an error apears:
error: "unresolved symbols remain"
undefined symbol: _ePWM
first reference in file: ../lib/SFO_TI_Build_V6b_FPU.lib<SFO_V6b.obj>
I couldn't finde the solution to this error.
Another question is: as I use 28069 device, which has floating-point unit, must I use only those libraries containing the "_FPU" ending? (like: rts2800_fpu32.lib, SFO_TI_Build_V6b_FPU.lib or IQmath_fpu32.lib)
Thanks,
Alex