Other Parts Discussed in Thread: INSTASPIN-BLDC, CCSTUDIO, DRV8312
Hello,
I have been using the InstSpin GUI for a while now, very successfully except for one issue: I have to give my motor (not the one with the kit) a slight push to get started and then it runs fine. To get around this I was hoping to use the hall sensors I have to get me started from zero.
So I switched to the PMSM/BLDC GUI which gives me the option of sensored versus sensorless control. It works fine for the motor that came with the kit. When I plug in my motor it seems to try and work for about 5 seconds. Current slowly ramps up and then comes to sudden halt. The motor either gets confused and then does a sudden jerk or it spins for the 5 seconds. No fault conditions arise the controller just stops pushing any current.
I did change two lines of code allowing the minimum Voltage to the motor to be +12V.
This GUI does not give me the option to change number of poles or frequency. Will I need to do that in the .c file? If so where?
Also I was wondering if there is an option to set what spacing / angles my hall sensors are set at (30 degrees)?
If there were a start from zero, feed forward type of option in the InstaSpin GUI that would be awesome!?
Thank you in advance for any help.
Matt