This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DPLib & ISR

Hello All,

I am exploring the DPLib and it's usage with the C2000 controllers.

I could gather from the Template Projects and the software for Development Tools (such as Solar DC-AC/ DC-DC kits)  that DPLib blocks are called in the ISR. However, the ISR is always an ASM file evidently because DPLib blocks are in ASM . However , is there a way to mix C and ASM code in ISR, thereby allowing me to use DPLib in ISR while still performing the rest of ISR operations in C ? If so, is there a sample project for this I could refer to ?

I am considering using the F28335 (which doesn't have explicit DPLib support). However, since I plan to use only the control utilities of DPLib, I am hoping they should directly port to F28335 as the assembly instructions shall remain the same. Any comments on this approach are welcome.

Thanks & Regards,

Jimit.