Other Parts Discussed in Thread: MOTORWARE, TMDSHVMTRINSPIN, CONTROLSUITE
Hello all,
We will use InstaSPIN-FOC MCU (F28027F) for our motor controller (our concern is for High Voltage 230V and 400V).
We will make controller device to control single phase motor and three phase motor (it will be two separate devices).
My questions are:
Is InstaSPIN-FOC (MotorWare) project can be used for single phase driver (to drive single phase motor)?
If yes, which parts of firmware modules should I concern about (ADC, PWM, etc)?
If no, which example project that I can use as reference for single phase motor?
What development kit I can refer to as reference design for single phase motor controller?
If any document that you can suggest, I appreciate it.
Thanks!
Best regards,
Maria