This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error connecting to the target from ccsv3.1 to board F2812



hi..i am newbie ..i have problem during connecting my program to the board F2812..before today is good but today i try to load my program the message appears:

Error connecting to the target: Error 0x80000200/-145 Fatal Error during: OCS,  Error generated by SD scan controller module  Sequence ID: 0 Error Code: -145 Error Class: 0x80000200

and this:

Error connecting to the target:
Error 0x80000200/-145
Fatal Error during: OCS,
Error generated by SD scan controller module

Sequence ID: 0
Error Code: -145
Error Class: 0x80000200
I/O Port = 378

Board Name: F2812 eZdsp
Cpu Name: cpu_0

Abort:        Close Code Composer Studio.
Retry:        Try to connect to the target again.
Cancel:        Remain disconnected from the target
Diagnostic:    Run diagnostic utility.

so..i dont no how to solve this problem..tq

  • Hi,

    Check these links out:

    http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/46697.aspx

    http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/265093/926613.aspx

    http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/105616.aspx

    Regards,

    Gautam

  • hi..i was test sd configuration..

    this messege appears:

    Spectrum Digital Configuration and Diagnostic Utility

    Supports:
    Printer Port: XDS510PP, XDS510PP+, SPI515, eZdsp
    ISA Bus:      SPI510, XDS510
    PCI Bus:      SPI525
    USB Bus:      XDS510-USB
    ** Checking for a valid emulator/eZdsp

      $$ You are connected to:
      $$ EmuProductName=XDS510PP_PLUS
      $$ EmuPortAddr=0x378
      $$ EmuPortMode=SPP8
      $$ ProductId=10
      $$ ProductVersion=84

      >> EmuProductName in sdopts.cfg does not match
      >> your connected emulator/eZdsp