Hi,
i'm using a F28334 chained with a lm3s828, connected via a XDS100v3. CCS5.1
When i try to debug a get the following error:
CORTEX_M3_0: GEL Output:
Memory Map Initialization Complete
CORTEX_M3_0: GEL Output: Watchdog Timer Enabled
CORTEX_M3_0: GEL Output: UARTs Enabled
C28xx: Flash Programmer: Missing Flash Programming Settings.
C28xx: Flash Programmer: Error erasing Flash memory.
C28xx: Flash Programmer: Missing Flash operation option. Operation cancelled.
C28xx: Trouble Writing Memory Block at 0x33d944 on Page 0 of Length 0x60
C28xx: GEL: File: F:\ ******.out: Load failed.
It turned out that the flash-settings options in the TARGET tab of the DebugCofiguration dissapeared for
the F28334 but they are still there for the lm3s828!
Do you know a possible root cause?
thanks in advance!
BR Harry