Hello- I have the experimenters kit with a F28027PTA chip on it.
I'm using Code Composer 3.3.81
I tried the first example in the tutorial - volume1 and get errors when I try to load the program from File>load
I am able to add files to the project.
The error I get is data verification failed at address 0x3FFFC0 Please verify target memory and memory map.
Thanks in advance for help!