HI.,
I am designing Intelligent Motor controller board for my project using concerto F28M36P63C2 MCU device.
my question is,
i need to add external flash for the booting concerto MCU.
what type of flash i can use(serial or parallel)
if serial can i use my configured UART or SSI other than default pins shown in boot configuration article in technical manual of F28M36X.any recommended chips for serial flashing?
if parallel what is the bus width(data and Address) i can use.any recommended chips?
my requirement is from flash MCU(both M3 and c28x) should boot and start running application without and other device support.
what is the maximum flash memory i can use?(i am planning for 4M/8M flash)
any design configuration methods are much appriciated.
i went through all documents and forum discussions i didn't got appreciable answer to my problem.