Other Parts Discussed in Thread: TMS320F28335
Hi
I ve attempting to program a TMS320F28335 experimenter Kit on Its flash memory , I've adjusted the Linker comand file .cmd as to load to the flash and run it from the RAM but it happens that when running from the compiler the led blinks but when I reset the CPU the led turns off, so the flash never gets programed.
Can some one explain the requiered steps to program the flash memory. I've guided on C200 delfino WorkShop> lab>10 without well results. I am using CSS v4.