Dear Folks,
I need to provide the analog input to the comparator1 of F28M36x device the technical reference manual or the datasheet doesn't clearly mention which pin is mapped to which input .They jut mention AIO_MUX1 and so on.
The output of the comparator is latched to the COMPSTS , Can I directly map it to GPIO of my interest without externally assigning the bit of COMPSTS to GPIO.
Regards,
Suresh Jaggal