This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5 failed to load Program in F28069

Hi,

I am using CCS 5.5 and my custom board F28069

I have imported  example bios project Flash Hello word for F28069 in CCS5.5 my custom board. While building project, there is no error or warning.

However while loading program to the controller , I get the  following erros:

C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: GEL: File: D:\TI_workspace_v5_5\fc3r3_test1\Debug\fc3r3_test1.out: Load failed.

What could be the  problem?

The program loads properly on CCS4.2.

I have also try to migrates program from CCS4.2 yo CCS5.5 but still error occurs at debugging.

Regs,

Naresh