Other Parts Discussed in Thread: CCSTUDIO
Hello,
I am trying to connect my eZdsp F28335 development board from Spectrum Digital with my Windows 8 computer.
I have followed the "Quick start installation guide" shipped with the eZdsp board, I have correctly installed the "CCS DSK v3.3 IDE" software and the "Drivers and Target Content" from the CD-ROM.
When I connect the eZdsp board with my computer the "new device installer wizard" of Windows automatically appears and it seems like he's installing drivers for 5-10 seconds. Unfortunately, when I look in the Device Manager there's a yellow symbol in front of the TMS320x28xx eZdsp and the Device Status is: "The drivers for this device are not installed. (Code 28)"
When I open the F28335 eZdsp CCStudio v3.3 there's also an error:
"Error initializing emulator
I/O Port = 540
Board Name: F28335_eZdsp
Cpu Name: cpu_0"
I don't use an external JTAG emulator. (Is this required?)
Do I need to install a more recent version of CCS?
Is there any way to let this F28335 eZdsp board work with Windows 8?
Thanks in Advance!
Pieter Gervoyse,
Master Student at the KU Leuven, Belgium