This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem while writing the eeprom on I2c

Other Parts Discussed in Thread: TMS320F28335

 

Hi,

I am trying to write the 100 bytes of data in EEprom. I am using EzDsp board. Controller am using is TMS320F28335. I just modified given sample code according to my apllication.

But still theri is problem after read of 16 bytes. As it is in FIFO mode and FIFO size is 16 bytes. But next time am sending new address but still their is problem .

Am sharing my code. Anyone can please suggest any solution.

 

 

#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

// Note: I2C Macros used in this example can be found in the
// DSP2833x_I2C_defines.h file

 

#define I2C_MAX_BUFFER_SIZE 63

// Prototype

 statements for functions found within this file.
void   I2CA_Init(void);
Uint16 I2CA_WriteData(struct I2CMSG *msg,Uint16);
Uint16 I2CA_ReadData(struct I2CMSG *msg,Uint16);
interrupt void i2c_int1a_isr(void);
//void pass(void);
//void fail(void);
void ReadData(void);
void WriteData(void);

#define I2C_SLAVE_ADDR        0x50
#define I2C_NUMBYTES          14
#define I2C_EEPROM_HIGH_ADDR  0x00
#define I2C_EEPROM_LOW_ADDR   0x30

// Global variables
// Two bytes will be used for the outgoing address,
// thus only setup 14 bytes maximum
struct I2CMSG I2cMsgOut1={I2C_MSGSTAT_SEND_WITHSTOP,
                          I2C_SLAVE_ADDR,
                          I2C_NUMBYTES,
                          I2C_EEPROM_HIGH_ADDR,
                          I2C_EEPROM_LOW_ADDR,
                                                               
      };

 

struct I2CMSG I2cMsgIn1={ I2C_MSGSTAT_SEND_NOSTOP,
                          I2C_SLAVE_ADDR,
                          I2C_NUMBYTES,
                          I2C_EEPROM_HIGH_ADDR,
                          I2C_EEPROM_LOW_ADDR};

struct I2CMSG *CurrentMsgPtr;    // Used in interrupts
Uint16 PassCount;
Uint16 FailCount;
Uint16 readcount;
Uint16 writecount;
Uint16 Error;


void main(void)
{
 Uint16 i;
  writecount=0;
  readcount=0;
 
   CurrentMsgPtr = &I2cMsgOut1;

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
   InitSysCtrl();


// Step 2. Initalize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio();
// Setup only the GP I/O only for I2C functionality
   InitI2CGpio();

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
   DINT;

// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
   InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
   IER = 0x0000;
   IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
   InitPieVectTable();

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
   EALLOW; // This is needed to write to EALLOW protected registers
   PieVectTable.I2CINT1A = &i2c_int1a_isr;
   EDIS;   // This is needed to disable write to EALLOW protected registers

// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
   I2CA_Init();

// Step 5. User specific code

   // Clear Counters
   PassCount = 0;
   FailCount = 0;

   // Clear incoming message buffer
   for (i = 0; i < I2C_MAX_BUFFER_SIZE; i++)
   {
       I2cMsgIn1.MsgBuffer[i] = 0x0000;
   }

// Enable interrupts required for this example

// Enable I2C interrupt 1 in the PIE: Group 8 interrupt 1
   PieCtrlRegs.PIEIER8.bit.INTx1 = 1;

// Enable CPU INT8 which is connected to PIE group 8
   IER |= M_INT8;
   EINT;

   // Application loop

 

 for(i=0;i<6;i++)
 {
 WriteData();
 }
 while(1)
 {

 ReadData();
 //DELAY_US(1000);
 

 }

}

void I2CA_Init(void)
{
   // Initialize I2C
   I2caRegs.I2CSAR = 0x0050;  // Slave address - EEPROM control code

   #if (CPU_FRQ_150MHZ)             // Default - For 150MHz SYSCLKOUT
        I2caRegs.I2CPSC.all = 14;   // Prescaler - need 7-12 Mhz on module clk (150/15 = 10MHz)
   #endif
   #if (CPU_FRQ_100MHZ)             // For 100 MHz SYSCLKOUT
     I2caRegs.I2CPSC.all = 9;     // Prescaler - need 7-12 Mhz on module clk (100/10 = 10MHz)
   #endif

   I2caRegs.I2CCLKL = 10;   // NOTE: must be non zero
   I2caRegs.I2CCLKH = 5;   // NOTE: must be non zero
   I2caRegs.I2CIER.all = 0x24;  // Enable SCD & ARDY interrupts

   I2caRegs.I2CMDR.all = 0x0020; // Take I2C out of reset
            // Stop I2C when suspended

   I2caRegs.I2CFFTX.all = 0x6000; // Enable FIFO mode and TXFIFO
   I2caRegs.I2CFFRX.all = 0x2040; // Enable RXFIFO, clear RXFFINT,

   return;
}


void WriteData(void)
{
 Uint16 i;
        Error = I2CA_WriteData(&I2cMsgOut1,writecount);
         // If communication is correctly initiated, set msg status to busy
         // and update CurrentMsgPtr for the interrupt service routine.
         // Otherwise, do nothing and try again next loop. Once message is
         // initiated, the I2C interrupts will handle the rest. Search for
         // ICINTR1A_ISR in the i2c_eeprom_isr.c file.
         if (Error == I2C_SUCCESS)
         {
            CurrentMsgPtr = &I2cMsgOut1;
            I2cMsgOut1.MsgStatus = I2C_MSGSTAT_WRITE_BUSY;
         }
  
 
  
}    


Uint16 I2CA_WriteData(struct I2CMSG *msg, Uint16 writecount)
{
   Uint16 i;
   // Wait until the STP bit is cleared from any previous master communication.
   // Clearing of this bit by the module is delayed until after the SCD bit is
   // set. If this bit is not checked prior to initiating a new message, the
   // I2C could get confused.
   if (I2caRegs.I2CMDR.bit.STP == 1)
   {
      return I2C_STP_NOT_READY_ERROR;
   }

   // Setup slave address
   I2caRegs.I2CSAR = msg->SlaveAddress;

   // Check if bus busy
   if (I2caRegs.I2CSTR.bit.BB == 1)
   {
      return I2C_BUS_BUSY_ERROR;
   }

   // Setup number of bytes to send
   // MsgBuffer + Address
   I2caRegs.I2CCNT = msg->NumOfBytes+2;

   // Setup data to send
   I2caRegs.I2CDXR = msg->MemoryHighAddr;
   I2caRegs.I2CDXR = msg->MemoryLowAddr + writecount;
// for (i=0; i<msg->NumOfBytes-2; i++)
   for (i=0; i<msg->NumOfBytes; i++)

   {
      I2cMsgOut1.MsgBuffer[i+writecount]= (i+writecount);
      I2caRegs.I2CDXR = *(msg->MsgBuffer+i+writecount);
   }

   // Send start as master transmitter
   I2caRegs.I2CMDR.all = 0x6E20;
   return I2C_SUCCESS;

}


   ///////////////////////////////////
      // Read data from EEPROM section //
   ///////////////////////////////////
void ReadData(void)
{
 
         // Check incoming message status.
         if(I2cMsgIn1.MsgStatus == I2C_MSGSTAT_SEND_NOSTOP)
         {
            // EEPROM address setup portion
            while(I2CA_ReadData(&I2cMsgIn1,readcount) != I2C_SUCCESS)
            {
               // Maybe setup an attempt counter to break an infinite while
               // loop. The EEPROM will send back a NACK while it is performing
               // a write operation. Even though the write communique is
               // complete at this point, the EEPROM could still be busy
               // programming the data. Therefore, multiple attempts are
               // necessary.
            }
            // Update current message pointer and message status
            CurrentMsgPtr = &I2cMsgIn1;
            I2cMsgIn1.MsgStatus = I2C_MSGSTAT_SEND_NOSTOP_BUSY;
  
         }
   
         // Once message has progressed past setting up the internal address
         // of the EEPROM, send a restart to read the data bytes from the
         // EEPROM. Complete the communique with a stop bit. MsgStatus is
         // updated in the interrupt service routine.
         else if(I2cMsgIn1.MsgStatus == I2C_MSGSTAT_RESTART)
         {
            // Read data portion
            while(I2CA_ReadData(&I2cMsgIn1,0) != I2C_SUCCESS)
            {
               // Maybe setup an attempt counter to break an infinite while
               // loop.
            }
            // Update current message pointer and message status
            CurrentMsgPtr = &I2cMsgIn1;
        I2cMsgIn1.MsgStatus = I2C_MSGSTAT_READ_BUSY;
         }
 
      }  // end of read section
  
}


Uint16 I2CA_ReadData(struct I2CMSG *msg, Uint16 readcount )
{
   // Wait until the STP bit is cleared from any previous master communication.
   // Clearing of this bit by the module is delayed until after the SCD bit is
   // set. If this bit is not checked prior to initiating a new message, the
   // I2C could get confused.

   if (I2caRegs.I2CMDR.bit.STP == 1)
   {
      return I2C_STP_NOT_READY_ERROR;
   }

   I2caRegs.I2CSAR = msg->SlaveAddress;

   if(msg->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP)
   {
      // Check if bus busy
      if (I2caRegs.I2CSTR.bit.BB == 1)
      {
         return I2C_BUS_BUSY_ERROR;
      }
      I2caRegs.I2CCNT = 2;
      I2caRegs.I2CDXR = msg->MemoryHighAddr;
      I2caRegs.I2CDXR = msg->MemoryLowAddr+readcount;
      I2caRegs.I2CMDR.all = 0x2620;   // Send data to setup EEPROM address
    
   }
   else if(msg->MsgStatus == I2C_MSGSTAT_RESTART)
   {
      I2caRegs.I2CCNT = msg->NumOfBytes; // Setup how many bytes to expect
      I2caRegs.I2CMDR.all = 0x2C20;   // Send restart as master receiver
   }

   return I2C_SUCCESS;
}

 


interrupt void i2c_int1a_isr(void)     // I2C-A
{
   Uint16 IntSource,i;

   // Read interrupt source
   IntSource = I2caRegs.I2CISRC.all;

   // Interrupt source = stop condition detected
   if(IntSource == I2C_SCD_ISRC)
   {
      // If completed message was writing data, reset msg to inactive state
      if (CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_WRITE_BUSY)
   {
  
  writecount= writecount+14;
     
      }
      else
      {
         // If a message receives a NACK during the address setup portion of the
         // EEPROM read, the code further below included in the register access ready
         // interrupt source code will generate a stop condition. After the stop
         // condition is received (here), set the message status to try again.
         // User may want to limit the number of retries before generating an error.
         if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY)
         {
            CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_SEND_NOSTOP;
         }
         // If completed message was reading EEPROM data, reset msg to inactive state
         // and read data from FIFO.
         else if (CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_READ_BUSY)
   
         {
   CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_SEND_NOSTOP;
                   for(i=0; i < I2C_NUMBYTES; i++)
            {
              CurrentMsgPtr->MsgBuffer[i+readcount] = I2caRegs.I2CDRR;
         }
   
         {
         // Check recieved data
         for(i=0; i < I2C_NUMBYTES; i++)
         {
            if(I2cMsgIn1.MsgBuffer[i+readcount] == I2cMsgOut1.MsgBuffer[i+readcount])
            {
                PassCount++;
            }
            else
            {
                FailCount++;
            }
  
         }

         if(PassCount == I2C_NUMBYTES)
    {
   readcount = readcount+14;
           // pass();
         }
         else
         {
           // fail();
         }


      }

    }
      }
   }  // end of stop condition detected

   // Interrupt source = Register Access Ready
   // This interrupt is used to determine when the EEPROM address setup portion of the
   // read data communication is complete. Since no stop bit is commanded, this flag
   // tells us when the message has been sent instead of the SCD flag. If a NACK is
   // received, clear the NACK bit and command a stop. Otherwise, move on to the read
   // data portion of the communication.
   else if(IntSource == I2C_ARDY_ISRC)
   {
      if(I2caRegs.I2CSTR.bit.NACK == 1)
      {
         I2caRegs.I2CMDR.bit.STP = 1;
         I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
      }
      else if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY)
      {
         CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_RESTART;
 
      }
   }  // end of register access ready

   else
   {
      // Generate some error due to invalid interrupt source
      asm("   ESTOP0");
   }

   // Enable future I2C (PIE Group 8) interrupts
   PieCtrlRegs.PIEACK.all = PIEACK_GROUP8;
}

/*void pass()
{
    asm("   ESTOP0");
    for(;;);
}

void fail()
{
    asm("   ESTOP0");
    for(;;);
}*/


//===========================================================================
// No more.
//===========================================================================