This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interrupts for c2000 in sumulink

Dear Folks,

I am using a hardware interrupt block and a function call to support when an interrupt occurs. My question is does the Simulink take care to clear the interrupt flags or do we need to clear them manually . I find that the function call is executed only once , when I re trigger the external interrupt I see no change. If we need to clear the interrupt flags externally could plz tell me how they have to cleared.

Regards,

Suresh Jaggal