Dear All,
We are using the command file F28069 which came with the Blinky LED example with our 28069 board and application. Our application has now grown to beyond 16K - however, the command file maps .text to FLASHA which is just below 16K long.
How can I modify the command file to accommodate larger programs and use the FLASHH to FLASHB memories defined in the command file?
Where can I find documentation on the command file structure for 28069?
Regards,
Vaidi.