Other Parts Discussed in Thread: CONTROLSUITE
----------------------------------------------------------------------------------------------------------------------------------------------------------
1. Develope Board : H52C1 Concerto Experimenter Kit
http://www.ti.com/tool/tmdsdockh52c1
2. Concerto F28M35x Technical Reference Manual
http://www.ti.com/lit/ug/spruh22f/spruh22f.pdf
6.6.9 C-Boot ROM MTOC IPC Commands
3. controlSUITE
C:\ti\controlSUITE\device_support\f28m35x\v201\MWare\driverlib
----------------------------------------------------------------------------------------------------------------------------------------------------------
Hi
I want to boot c28 by using "C-Boot ROM MTOC IPC Commands" referenced form "Concerto F28M35x TRM - 6.6.9 "
So I make code m3 side that below add.
----------------------------------------------------------------------------------------------------------------------------------------------------------
... some intialize code first
// Define Local Variables
unsigned short ErrorCount = 0;
unsigned short usWWord16;
unsigned short *pWord16;
unsigned long ulWWord32;
unsigned long *pWord32;
unsigned short usRWord16;
unsigned long ulRWord32;
unsigned long *pulMsgRam;
unsigned long ulAddress=0;
unsigned int i,j,k,m,n;
unsigned char *pc;
ErrorFlag = 0;
usWWord16 = 0x1234;
ulWWord32 = 0xABCD5678;
usRWord16 = 0;
ulRWord32 = 0;
//-------------------------------------------------------------------------------------------------------
RAMControlInitM1MsgRam();// defined ram.h
RAMControlInitL0L3Ram();
//-------------------------------------------------------------------------------------------------------
UART_printf("sizeof(bootloader_c28)= %d\n\n",sizeof(bootloader_c28));
ulAddress=0x00;
for(i=0,k=0; i<(sizeof(bootloader_c28)/2); ++i,++ulAddress, k+=2)
{
pWord16=&bootloader_c28[k];
IPCLiteMtoCDataWrite(IPC_FLAG1, ulAddress,(unsigned long)(*pWord16), IPC_LENGTH_16_BITS, IPC_FLAG32);
UART_printf("IPCLiteMtoCDataWrite: 0x%x = \t0x%x\n",ulAddress,(*pWord16));
//SimpleDelay();
while (IPCLiteMtoCGetResult(&usRWord16, IPC_LENGTH_16_BITS, IPC_FLAG32) != STATUS_PASS)
{
}
if ((*pWord16) != usRWord16)
{
ErrorCount++;
UART_printf("\tError #1\n");
}
UART_printf("\tIPCLiteMtoCGetResult: \t0x%x\n",usRWord16);
usRWord16 = 0;
UART_printf("IPCLiteMtoCDataRead: 0x%x\n",ulAddress);
while (IPCLiteMtoCDataRead(IPC_FLAG1, ulAddress, IPC_LENGTH_16_BITS, IPC_FLAG32) != STATUS_PASS)
{
}
// Result of Read will be read into usRWord16 variable.
while (IPCLiteMtoCGetResult(&usRWord16,IPC_LENGTH_16_BITS, IPC_FLAG32) != STATUS_PASS)
{
}
if ((*pWord16) != usRWord16)
{
ErrorCount++;
UART_printf("\tError #2\n");
}
UART_printf("\tIPCLiteMtoCGetResult: \t0x%x\n\n",usRWord16);
SimpleDelay();
}
----------------------------------------------------------------------------------------------------------------------------------------------------------
Result from UART
----------------------------------------------------------------------------------------------------------------------------------------------------------
sizeof(bootloader_c28)= 760
IPCLiteMtoCDataWrite: 0x0 = 0x40
IPCLiteMtoCGetResult: 0x40
IPCLiteMtoCDataRead: 0x0
IPCLiteMtoCGetResult: 0x40
IPCLiteMtoCDataWrite: 0x1 = 0x3af
IPCLiteMtoCGetResult: 0x3af
IPCLiteMtoCDataRead: 0x1
IPCLiteMtoCGetResult: 0x3af
IPCLiteMtoCDataWrite: 0x2 = 0x3af
IPCLiteMtoCGetResult: 0x3af
IPCLiteMtoCDataRead: 0x2
IPCLiteMtoCGetResult: 0x3af
IPCLiteMtoCDataWrite: 0x3 = 0x0
IPCLiteMtoCGetResult: 0x0
IPCLiteMtoCDataRead: 0x3
IPCLiteMtoCGetResult: 0x0
IPCLiteMtoCDataWrite: 0x4 = 0x761b
IPCLiteMtoCGetResult: 0x761b
IPCLiteMtoCDataRead: 0x4
Error #2
IPCLiteMtoCGetResult: 0x1
IPCLiteMtoCDataWrite: 0x5 = 0xfff0
IPCLiteMtoCGetResult: 0xfff0
IPCLiteMtoCDataRead: 0x5
IPCLiteMtoCGetResult: 0xfff0
IPCLiteMtoCDataWrite: 0x6 = 0xe200
IPCLiteMtoCGetResult: 0xe200
IPCLiteMtoCDataRead: 0x6
Error #2
IPCLiteMtoCGetResult: 0x7
IPCLiteMtoCDataWrite: 0x7 = 0xbd
IPCLiteMtoCGetResult: 0xbd
IPCLiteMtoCDataRead: 0x7
Error #2
IPCLiteMtoCGetResult: 0x0
IPCLiteMtoCDataWrite: 0x8 = 0xe630
IPCLiteMtoCGetResult: 0xe630
IPCLiteMtoCDataRead: 0x8
IPCLiteMtoCGetResult: 0xe630
...
...
IPCLiteMtoCDataWrite: 0x2d = 0xfff0
IPCLiteMtoCGetResult: 0xfff0
IPCLiteMtoCDataRead: 0x2d
IPCLiteMtoCGetResult: 0xfff0
IPCLiteMtoCDataWrite: 0x2e = 0xe200
IPCLiteMtoCGetResult: 0xe200
IPCLiteMtoCDataRead: 0x2e
Reboot hear and repeat first code
sizeof(bootloader_c28)= 760
IPCLiteMtoCDataWrite: 0x0 = 0x40
IPCLiteMtoCGetResult: 0x40
IPCLiteMtoCDataRead: 0x0
IPCLiteMtoCGetResult: 0x40
IPCLiteMtoCDataWrite: 0x1 = 0x3af
IPCLiteMtoCGetResult: 0x3af
IPCLiteMtoCDataRead: 0x1
IPCLiteMtoCGetResult: 0x3af
...
...
----------------------------------------------------------------------------------------------------------------------------------------------------------
Question
1. Why the writed value is different at adress 0x04, 0x06, 0x07 ?
My code is really wirte c28 ram adress 0x00000 ?
2. Why reboot at adress 0x2e ?
Thank you for reading and i really need your help!